Hello,
once u-boot determines with hab_auth_img() that signed kernel image is correct and signed dtb file is correct , which is the correct command to launch that kernel image ? is it needed to extract the start address from boot data table or is there already a command for this ?
And for the dtb ?
thank you
Hello,
You may look at bootcmd command of U-boot in its environment.
Have a great day,
Yuri.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.