HDMI RX or HDMI-IN on imx8qm-mek with Android 9 Auto

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HDMI RX or HDMI-IN on imx8qm-mek with Android 9 Auto

Jump to solution
1,713 Views
amit251291
Contributor IV

Dear all,

We are working on imx8qm-mek running on Android 9 - auto. I have gone through the couple of posts from this forum regarding HDMI-RX functionality. 

I have used fsl-imx8qm-mek-hdmi-in.dts as reference and modified fsl-imx8qm-mek-car.dts. After flashing completed build on MEK platform  i am receiving below log. 

[ 4.424144] [drm:hdmirx_init] *ERROR* NO HDMI RX FW running
[ 4.429740] mxc-hdmi-rx 58268000.hdmi_rx: mxc hdmi rx init failed
s[ 4.435919] mxc-hdmi-rx 58268000.hdmi_rx: mxc hdmi rx probe failed

So here i see that HDMI RX FW is not running and so the error is thrown. 

I found the firmware are locate here : 

vendor/nxp/linux-firmware-imx/firmware/hdmi/cadence/hdmirxfw.bin 

vendor/nxp-opensource/imx-mkimage/iMX8QM/hdmirxfw.bin

I need to understand how i can use these firmware to resolve the above issue ? It will be great if someone can throw some light here. 

0 Kudos
Reply
1 Solution
1,514 Views
igorpadykov
NXP Employee
NXP Employee

Hi Amit

image should have correct signed HDMI RX firmware, however according

to p.21 i.MX 8QuadMax Automotive and Infotainment Applications Processors

currently HDMI RX is not supported, relevant software and documentation may be provided later

after validation.

pastedImage_1.jpg

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
1,515 Views
igorpadykov
NXP Employee
NXP Employee

Hi Amit

image should have correct signed HDMI RX firmware, however according

to p.21 i.MX 8QuadMax Automotive and Infotainment Applications Processors

currently HDMI RX is not supported, relevant software and documentation may be provided later

after validation.

pastedImage_1.jpg

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,483 Views
nhermann
Contributor I

Dear Igor, what is the current status of HDMI Rx?

Best regards

Nikolaj

0 Kudos
Reply
1,514 Views
amit251291
Contributor IV

Thank you  igorpadykov‌ for your response. 

0 Kudos
Reply