Hi,
I want to install "MPC8272ADS_20080623-ltib" on my Fedora 10 distrib. I use the following installation process:
- mount -o loop MPC8272ADS_20080623-ltib.iso /mnt
- /mnt/install
- I follow setup process
After installation directory ltib-mpc8272ads-20080623 is created but there are nothings created in opt/ directory.
When I launch ./ltib, I have the following error :
"ltib cannot be run because one or more of the host packages needed
to run it are either missing or out of date.
Please install/upgrade these packages and then re-try.
Package Minimum ver Installed info
------- ----------- ---------------
rpm-build 0 not installed
Died at ./ltib line 1241.
traceback:
main::host_checks:1241
main:489
Started: Wed Apr 8 10:51:43 2009
Ended: Wed Apr 8 10:51:45 2009
Elapsed: 2 seconds
Build Failed
Exiting on error or interrupt"
Is there somethings wrong in the manner I make installation ?
Is it normal there are no directory created in opt/ ?
I'm having this same issue. Did anybody find a solution? It's very annoying after
all the other packages I had to install to be held up by just this one problem.
From the directory where you type "./ltib" type "gedit ltib" if you have a Gnome install. I'm not sure what the KDE editor is, or use VI if you want edit in the console text mode. Search for "pre_install_deps". This is the table that "check_basic_deps" refers to. Look for a line that contains " rpm-buld 0". Comment out the line by adding "#" to the left of the line. Save and you should be good to go.
Same problem onto the MPC8313, details below:
I want to install "ltib-mpc8313erdb-20081222" on my Fedora 10 distrib. I use the following installation process:
- mount -o loop MPC8313E_RDB_K26_20081226-LTIB.iso /mnt/
- cd /mnt/install
- I follow setup process, it ends successfully
When I launch ./ltib or ./ltib -c , I have the following error :
ltib cannot be run because one or more of the host packages needed
to run it are either missing or out of date.
Please install/upgrade these packages and then re-try.
Package Minimum ver Installed info
------- ----------- ---------------
rpm-build 0 not installed
Died at ./ltib line 1241.
traceback:
main::host_checks:1241
main:489
Started: Sun Jun 14 08:33:16 2009
Ended: Sun Jun 14 08:33:19 2009
Elapsed: 3 seconds
Build Failed
Exiting on error or interrupt
$ rpmbuild --version
RPM version 4.6.1
Same problem with OpenSuse 11.1
Can you confirm you have rpm-build installed? (rpm -q rpm-build).
In case you have, then probably a good idea is to post this into the LTIB mailing list:
Ltib mailing list
Ltib@nongnu.org
http://lists.nongnu.org/mailman/listinfo/ltib
Regards,
Fabio Estevam
I have same issue on Fedora 11. when I runt the command ->rpm -q rpm-build, it shows->
rpm-build-4.7.0-1.fc11.i586
Do you have solution for this?