Flash u-boot-nand.imx to NAND

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash u-boot-nand.imx to NAND

1,226 Views
jupiter_hce
Contributor III

Hi,

I am running a customized iMX6ULZ EVK, I am able to use kobs-ng to flash u-boot-nand.imx to NAND in Linux, has anyone used u-boot command to flash u-boot-nand.imx to NAND in u-boot instead? Or is it possible to flash u-boot-nand.imx to NAND in u-boot? Is any iMX6 document to flash u-boot-nand.imx to NAND in u-boot?

Thank you.

- jupiter

Labels (4)
Tags (1)
0 Kudos
Reply
1 Reply

1,033 Views
igorpadykov
NXP Employee
NXP Employee

Hi jupiter

nxp does not support such operations in uboot, in general one can look

at mainline uboot resources (sect.7.6. Boot from NAND Flash Memory):

Manual < DULG < DENX 

[U-Boot] [PATCH 3/3] i.MX: nand: add nandbcb update command 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply