Please tell me about uuu.
I tried to burn image for i.mx6q board by uuu, but It is a situation that is stopped in the following situation.
>uuu -b emmc_all bootloader rootfs.sdcard.bz2/*
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.3.102-0-gb078bd0 Success 0 Failure 0 1:2 1/ 1 [=================100%=================] SDP: boot -f u-boot-sd-2017.03-r0.imx
Could you give me any instructions?
Hi Aldo,
Thank you for advice.
I tried to burn image by MFGTool before, but it is not corresponded with USB3.0 port, so I can't.
I'm using L4.9.88. Looking at the link below, UUU is compatible with 4.9.88, so I tried it.
https://community.nxp.com/message/1200364?commentID=1200364#comment-1200364
Best regards
Hello,
Unfortunately by default it is not supported since UUU needs to have fastboot enabled in uboot, you may need to generate custom script, like in this case:
https://github.com/NXPmicro/mfgtools/issues/46
Hope this helps,
Best regards,
Aldo.
Hello,
If using an older BSP, equal or lower than L4.9.88_2.0.0, don't support UUU you may use old MFGTool for this case.
For the uboot version I believe you're using L4.9.11 right?
You may download MFGTool from here:
i.MX Series Manufacturing Toolkit for Linux 4.9.11_1.0.0 Release
Hope this helps,
Best regards,
Aldo.