USB no longer builds with MCUXpresso SDK 2.7.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB no longer builds with MCUXpresso SDK 2.7.0

870 Views
jeffthompson
Contributor V

I upgraded from MCUXpresso SDK 2.6.2. to 2.7.0 and now usb_usrt_drv.c fails to compile because fsl_uart,h is missing and many definitions like uart_handle_t, UART_TYPE, UART_BASE_PTRS, and others along with it. Is there an updated usb_uart_drv.c?

Labels (1)
0 Kudos
Reply
3 Replies

767 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello Jeff Thompson

 

The driver for the uart is called fsl_lpuart. Also the uart.h can be found at the components folder. You can drag these files from the sdk folder to your project.

pastedImage_2.png

 

If you have more questions do not hesitate to ask me.

Best regards,

Omar

0 Kudos
Reply

767 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello Jeff Thompson

Can you help me providing me the part number of the device you are working with?

Best regards,

Omar

0 Kudos
Reply

767 Views
jeffthompson
Contributor V

Omar,

It’s the MIMXRT1062DVL6A.

Jeff Thompson | Senior Electrical Engineer-Firmware

+1 704 752 6513 x1394

www.invue.com

0 Kudos
Reply