Hi,
IMX8M Mini consists of 4 CPUs Cortex A53 + 1 Micro Cortex M4.
I would like to know the total mcps supported by IMX8M Mini.
Is it 1800 + 400 MHz or 1800*4 + 400MHz.
Each CPU provides 1800 Mhz? or all together adds upto 1800 Mhz + 400 Mhz for micro.
We want to run some programs in different CPU in parallel. Could you please let me know.
Thank you, Sreedhar
i.MX8MM has up to 4 A53 running at up to 1800MHz and single M4 cores running at 400MHz.
All they can run in parallel.
Hi Victor Linnik,
Thank you for the answer.
Could you please clarify me:
Each CPU provides 1800 Mhz (4 * 1800 = 7200)? or all together adds upto 1800 Mhz
and 400 Mhz for micro
Thank you, Sreedhar
Yes. One may say that there are 7200 total Mhz for A53 cores and 400 Mhz in addition.
All these cores can run in parallel.
Thank you Victor Linnik