Hello everyone!
I'm having problems with the MCF5441X family of microcontrollers with some Processor expert libraries.
The high level components (BITIO, TIMERs, etc...) get an error called: "This component is not implemented in this version yet!" and I can't start programming with the Professor expert tool.
Can you help me? I attach a picture
Good morning, sir.
I explain: Any high level component of the processor expert is not compatible with the MCF54418. I need to use these libraries to control 2 external components: an AD9826 to convert video images and a sensor that works with clock signals. I am enclosing what I have on my project but I would like you to offer help as soon as possible.
Another issue is that I need libraries to control a NAND RAM memory and another DDR2 (MT29F2G08ABA and
MT47H128M8CF-3 IT respectively).
Thank you very much.
Hi Juan,
Please check my feedback at Case: 00242273. Thanks.
Have a great day,
Mike
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Ok mike, thanks for all
De: Hui_Ma
Enviado el: jueves, 28 de noviembre de 2019 7:54
Para: Juan Luis Lopez García
Asunto: Re: - Re: BITIO with MCF5441X
NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
Re: BITIO with MCF5441X
reply from Hui_Ma<https://community.nxp.com/people/Hui_Ma?et=watches.email.thread> in ColdFire/68K Microcontrollers and Processors - View the full discussion<https://community.nxp.com/message/1238764?commentID=1238764&et=watches.email.thread#comment-1238764>
Hi,
I am checking this issue with CodeWarior software team.
I will update when there with any feedback.
Thanks for the patience.
Have a great day,
Mike
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------