I am using the MIMXRT1064-EVK for a project that involves using the SPI on the board. When looking through the schematics there is a DNP on the ports for the SPI clock, MOSI, MISO, and CS. Is there anyway to get around this or do I need to use a different board. Also does anybody have SPI user notes?
Hi
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
The R278, R279, R280, R281 are not mounted on the MIMXRT1064-EVKboard actually, to use the LPSPI interface, you should weld 0Ω resistor to R278, R279, R280, R281.
Hope this is clear.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------