hello,Community
It is used as a start signal for PMIC with externally connected PMIC_ON_REQ pin.
Can the PMIC_ON_REQ pin be set to low by software when it is in the ON state?
If I can set the PMIC_ON_REQ pin low by software, which register should I control?
best regards
Goto
Hi Goto
>Can the PMIC_ON_REQ pin be set to low by software when it is in the ON state?
yes. One can look at patch provided on Q&A: How is mx6 PMIC_ON_REQ under SW control?
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------