How to use the NFC cockpit with PN7150

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use the NFC cockpit with PN7150

1,110 Views
ahmedmomar88
Contributor I

Hi, I am new to NFC and I have a question: Can I use the NFC cockpit with the PN7150 NFC controller? And how can I do so? e.g. using which board, which library..?

It is mentioned that the cockpit only works with PN7462 all-in-one or some other front-ends, but can it work with the PN7150?

Tags (2)
0 Kudos
Reply
2 Replies

969 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

 Yes, The NFC cockpit can't support PN7150. One may find the detail information as the link. NFC Cockpit | NXP .

Hope it help you. 

Best regards

0 Kudos
Reply

969 Views
hanraaijmakers
NXP Employee
NXP Employee

A pitty. Looks like a nice application and there are small PN7150 USB interfaced boards available now.

0 Kudos
Reply