I'm looking at using the MKV31512VLH12 microcontroller and am curious if the component has 5V tolerant I/O. I can't seem to find anything on the datasheet.
Hi Kyle, I hope you're doing well!
The KV31F's Maximum Digital Input Voltage value is (Vdd + 0.3V), and the Maximum Digital Output Voltage is (Vdd - 0.5). The operating ranges for Vdd is from -0.3V to a Maximum of 3.8V.
For more information about the operating characteristics of the KV31F, you can check its datasheet, here.
Please let me know if you have any other questions.
Best regards,
Sebastian