Build Error because of S32 Design Studio for Power (MBD Tool MPC57xx)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Build Error because of S32 Design Studio for Power (MBD Tool MPC57xx)

Jump to solution
1,221 Views
abhishek_kumar1
Contributor IV

I have MATLAB 2018b. 

I installed Design Studio for Power 2.1 and suddenly Simulink file do not build anymore 

I changed the registry value (below)

pastedImage_1.png

 I have attached the error and build file. 

 

mariuslucianandrei

Tags (1)
1 Solution
1,099 Views
mariuslucianand
NXP Employee
NXP Employee

Hi abhishek.kumar@chassisbrakes.com‌,

There are some differences in the folder structure, between the S32DS for PA 2.1 vs 2017.R1, so, in order to build using the compiler from S32DS V2.1, the following changes must be performed:

   1. S32DS_PA_TOOL must be set as path variable as 'C:\NXP\S32DS_Power_v2.1'

   2. the .tmf file from src\mbdtbx_mpc574x\mbdtbx_mpc574x location must be updated with the one attach. 

Best Regards,

Marius

View solution in original post

1 Reply
1,100 Views
mariuslucianand
NXP Employee
NXP Employee

Hi abhishek.kumar@chassisbrakes.com‌,

There are some differences in the folder structure, between the S32DS for PA 2.1 vs 2017.R1, so, in order to build using the compiler from S32DS V2.1, the following changes must be performed:

   1. S32DS_PA_TOOL must be set as path variable as 'C:\NXP\S32DS_Power_v2.1'

   2. the .tmf file from src\mbdtbx_mpc574x\mbdtbx_mpc574x location must be updated with the one attach. 

Best Regards,

Marius