Hello,
I am now learning how to configurate a FlexRay cluster by using MC9S12XF512. My node has successfully joined a two nodes FlexRay cluster (There exists a configurated FlexRay network). In this cluster, my node can receive the message that the other two nodes communicate. But when I try to create a FlexRay network between my node and any one of the existed FlexRay node separately, it will be failed. That is means, when the FlexRay network is activated, my node can join in the network and work properly. However, my node can not activate a FlexRay network.
I have set my node as a coldstart node in Fr_HW_cfg_00. And it also work when I configurate a FlexRay network with two MC9S12XF512 node.
The problem may be that I don't set a synchronously method for this node (TT-L, TT-D or TT-E), I have not found where can I set this parameter. Is there anyone konw this part?
Below is the Fr_HW_cfg and Fr_low_level_cfg
const Fr_HW_config_type Fr_HW_cfg_00 =
{
0x000400, // FlexRay module base address
0x0FF000,//0x0FF000 // FlexRay memory base address (MB headers start at this address)
FR_MC9S12XF, // Type of Freescale FlexRay module
FALSE, // Synchronization filtering
//FR_EXTERNAL_OSCILLATOR,
FR_INTERNAL_SYSTEM_BUS_CLOCK,
0, // Prescaler value
16, // Data size - segment 1
8, // Data size - segment 2
10, // Last MB in segment 1 (Number of MB in Segment1 - 1)
18, // Last individual MB (except FIFO); (Number of MB in Segment1 + Number of MB in Segment2 - 1)
29, // Total number of used MB (Last_individual_MB + 1 + FIFO)
TRUE, // Allow coldstart
0, // The value of the TIMEOUT bit field in the SYMATOR register - not implemented for all FlexRay modules
0, // Offset of the Sync Frame Table in the FlexRay memory
FR_DUAL_CHANNEL_MODE // Single channel mode disabled
};
const Fr_low_level_config_type Fr_low_level_cfg_set_00 =
{
10, /* G_COLD_START_ATTEMPTS */
5, /* GD_ACTION_POINT_OFFSET */
91, /* GD_CAS_RX_LOW_MAX */
0, /* GD_DYNAMIC_SLOT_IDLE_PHASE */
14, /* GD_MINISLOT */
5, /* GD_MINI_SLOT_ACTION_POINT_OFFSET */
65, /* GD_STATIC_SLOT */
0, /* GD_SYMBOL_WINDOW */
15, /* GD_TSS_TRANSMITTER */
59, /* GD_WAKEUP_SYMBOL_RX_IDLE */
50, /* GD_WAKEUP_SYMBOL_RX_LOW */
301, /* GD_WAKEUP_SYMBOL_RX_WINDOW */
180, /* GD_WAKEUP_SYMBOL_TX_IDLE */
60, /* GD_WAKEUP_SYMBOL_TX_LOW */
2, /* G_LISTEN_NOISE */
5000, /* G_MACRO_PER_CYCLE */
2, /* G_MAX_WITHOUT_CLOCK_CORRECTION_PASSIVE */
2, /* G_MAX_WITHOUT_CLOCK_CORRECTION_FATAL */
22, /* G_NUMBER_OF_MINISLOTS */
62, /* G_NUMBER_OF_STATIC_SLOTS */
4985, /* G_OFFSET_CORRECTION_START */
17, /* G_PAYLOAD_LENGTH_STATIC */
5, /* G_SYNC_NODE_MAX */
0, /* G_NETWORK_MANAGEMENT_VECTOR_LENGTH */
TRUE, /* G_ALLOW_HALT_DUE_TO_CLOCK */
20, /* G_ALLOW_PASSIVE_TO_ACTIVE */
FR_CHANNEL_AB, /* P_CHANNELS */
1875, /* PD_ACCEPTED_STARTUP_RANGE */
3, /* P_CLUSTER_DRIFT_DAMPING */
72, /* P_DECODING_CORRECTION */
6, /* P_DELAY_COMPENSATION_A */
6, /* P_DELAY_COMPENSATION_B */
401202, /* PD_LISTEN_TIMEOUT */
601, /* PD_MAX_DRIFT */
0, /* P_EXTERN_OFFSET_CORRECTION */
0, /* P_EXTERN_RATE_CORRECTION */
24, /* P_KEY_SLOT_ID */
TRUE, /* P_KEY_SLOT_USED_FOR_STARTUP */
TRUE, /* P_KEY_SLOT_USED_FOR_SYNC */
1392, /* P_KEY_SLOT_HEADER_CRC */
21, /* P_LATEST_TX */
7, /* P_MACRO_INITIAL_OFFSET_A */
7, /* P_MACRO_INITIAL_OFFSET_B */
2, /* P_MICRO_INITIAL_OFFSET_A */
2, /* P_MICRO_INITIAL_OFFSET_B */
200000, /* P_MICRO_PER_CYCLE */
241, /* P_OFFSET_CORRECTION_OUT */
601, /* P_RATE_CORRECTION_OUT */
FALSE, /* P_SINGLE_SLOT_ENABLED */
FR_CHANNEL_A, /* P_WAKEUP_CHANNEL */
30, /* P_WAKEUP_PATTERN */
40, /* P_MICRO_PER_MACRO_NOM */
8 /* P_PAYLOAD_LENGTH_DYN_MAX */
};
Hello Chen,
I have received some information from our expert, please, see the points below:
In case of your node is able to synchronize into the running FlexRay cluster, then it has to be able to coldstart cluster as well. I would recommend to check that all nodes in the cluster are configured to be a coldstartes.
In case of all nodes in your cluster are configured to be coldstarters, then it does not depend on order in which nodes are starting.
In case of there is only one coldstarter, then other (non-coldstarter) nodes must be started prior the colstarter node (they will wait in the integration listen state for the coldstarter).
In case of starting sequence is different and coldstarter node is waiting, then synchronization will not start.
I hope it helps you.
Best Regards,
Diana