Hi ,
I want to add cluster GROUP SERVER with AN-1217 END DEVICE.
here is the process that I followed.
Hi,
I am not sure, why are you trying to set the Group as Server?
However, I recommend that this management process be implemented in a router or Coordinator.
The bus error A bus error exception is generated when software attempts to access a memory address that does not exist or is not populated with memory or peripheral registers.
Could you please try with the max number of Groups 8?
Regards,
Mario
Hi,Mario.
I want to develop a light that needs to enter sleep mode,but I notice that the router can not enter sleep mode.
I tried to modify the max number of Group 8(even 1),it still had same question.
Or maybe the router can enter sleep mode? Is there an docement to refer?
Thank!
Hi Jiazhao,
We do not recommend that the router enters in sleep mode. The router is saving data(routing tables) for the Zigbee network. Instead, you could use the sleep end device and set some time for the wakeup.
Regards,
Mario
Hi Mario.
I had found out the reason that cause the error.I did not define Group Address Table in app.zpscfg.
Thank for you help!