LPC54608
MDK + JLINK
程序编译完成后能下载运行且正常;
但是debug有问题,一点debug就自动运行并且跑飞。这时候reset后,可以进入main函数,但是仿真(F11)没几步就出错。
LPC54608 MDK + JLINK SWD
I can download my code to the MCU and it works correctly, but i can't debug it.
I also can't debug the SDK demo project.
When I debug it, the mcu enters a "error run state". Below is 2 pictrues about it.
Then i click "Stop", the IDE shows
Then I click "OK", the IDE shows
Then I click "OK", the IDE exits the Debug Mode.
Help me !
Hello,
What about your project ?
How about debug the SDK demo project ?
BR
Alice