Hello,
I would like to ask if the following PHYs will work with LS1043A as replacement for the RGMII and SGMII PHYs.
If not, what Ethernet PHYs could I use other than the ones specified in the RDB?
Thank you very much.
Best,
Carlos
Please be aware, that we do not test third-party Ethernet PHYs
against our processors and do not keep an officially "approved" PHY
list. Instead, we emphasize on the compatibility of MAC/PHY interfaces
of our processors to the respective standard specifications to
allows our customers to have the maximum wide choice of third-party
components. Our response to your inquiry therefore is, you can use
your PHY devices al long as they satisfy the requirements of the
supported interface between the MAC and the PHY and the requirements
of the processor Datasheet.
Regards,
Platon
Thank you, bpe.
Best,
Carlos