MIPI_CSI Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIPI_CSI Error

776 Views
santhosh2
Contributor IV

Hi,

I have connected the Camera to MIPI_CSI and when i run the gstreamer command I'm getting the below error

root@iWave-G27M:~#export DISPLAY=:0
root@iWave-G27M:~# gst-launch-1.0 v4l2src device=/dev/video0 ! video/x-raw ! videoconvert ! ximagesink
Setting pipeline to PAUSED ...
Pipeline [i s2 5l6i2v.e5 3a7n7d9 7do]e sm xnco_tis nie.e0d:  PCRaEnR'OtL Lf i.n.d. s
Suebtdteivng
 pipeline to PLAYING ...
New clock: GstSystemClock
[ 2562.550871] mxc_isi.0: Can't find subdev
[ 2562.555044] mxc_isi.0: Can't find subdev
[ 2562.559245] mxc_isi.0: Can't find subdev
[ 2562.563423] mxc_isi.0: Can't find subdev
[ 2562.567575] mxc_isi.0: Can't find subdev
[ 2562.571731] mxc_isi.0: Can't find subdev
[ 2562.575859] mxc_isi.0: Can't find subdev
[ 2562.581833] (null): mxc_isi_source_fmt_init, No remote pad found!
[ 2562.587971] bypass csc
[ 2562.590340] input fmt RG10
[ 2562.593079] output fmt YUYV
[ 2562.595910] mxc-isi 58100000.isi: input_size(0,0), output_size(200,320)
[ 2562.602575] mxc_isi.0: Can't find subdev
^Chandling interrupt.
Interrupt: Stopping pipeline ...
Execution ended after 0:00:03.765367869
Setting pipeline to PAUSED ...
Setting pipeline to READY ...
Setting pipeline to NULL ...
Freeing pipeline ...
root@iWave-G27M:~#

Let me know how can i resolve

Regards

0 Kudos
Reply
1 Reply

573 Views
igorpadykov
NXP Employee
NXP Employee

Hi Santhosh

seems you are using third party board which is supported by its vendor,

issue may be posted on its support forum

https://www.iwavesystems.com/imx8-quadmax-smarc-som.html 

alternatively one can try with nxp reference boards and software:

i.MX Software | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply