Hello, everybody.
I want to change u-boot's Config from SD Card to NAND.
However, an error will occur even if you proceed as shown in the manual and the following link.
* manual name = i.MX_Yocto_Project_User's_Guide_Linux.pdf (attached)
* Follow Link = http://cache.freescale.com/files/training/doc/ftf/2014/FTF-SDS-F0106.pdf
The error content is as follows:
---------------------------------------------------------------------------------------------------------------------------------------------------------------
test@test-VirtualBox:~/fsl-release-bsp$ MACHINE=imx6qsabresd source setup-environment test_pms/
test@test-VirtualBox:~/fsl-release-bsp/test_pms$ bitbake -c deploy u-boot-imx
Loading cache: 100% |##########################################################################################################################| ETA: 00:00:00
Loaded 2211 entries from dependency cache.
ERROR: Nothing PROVIDES 'u-boot-imx'
ERROR: u-boot-imx was skipped: You cannot use UBOOT_MACHINE and UBOOT_CONFIG at the same time.
ERROR: u-boot-imx was skipped: UBOOT_CONFIG nand is not supported
ERROR: u-boot-imx was skipped: UBOOT_CONFIG nand is not supported
Summary: There was 1 ERROR message shown, returning a non-zero exit code.
---------------------------------------------------------------------------------------------------------------------------------------------------------------
Do I need to do something else before I follow the manual?
The manual only says that UBOOT_CONFIG should be modified as follows: UBOOT_CONFIG = "nand"
I confirmed that my kernel and dtb were working successfully (made according to the manual).
But only u-boot can't change to NAND...
The version of u-boot I use is confirmed to be v2014.01-r0.
(The version of u-boot that is currently created.)
We need your help!
pls refer to the topic as below:
https://community.nxp.com/message/438052?commentID=438052#comment-438052
Dear Joan Xie
Thank you for your reply.
Also, thank you for providing me with the necessary information in the future.
However, when UBOOT_CONFIG = "nand" was applied, the reason for the error could not be determined.
It also failed to determine how to resolve the error.
When I follow your link, it appears that UBOOT_MACHINE and UBOOT_CONFIG are not available at the same time.
Does UBOOT_CONFIG = "nand" require a different procedure?
I need your help.