IMXRT1021CAF4A仿真器死活连不上大概是什么原因?仿真器用的是JLINK,XpressoIDE版本是10.3.1 2233。
芯片供电电压,内核1.1电压都正常。
这是JTAG/SWD部分的电路图。
其中,JTRST信号也就到POR口了,如下图:
不知原理部分是由问题吗?我采用SWD方式连接。
工程设置如下:
startup配置:
提示错误信息:
Hi yi wan ,
非常感谢使用NXP产品,很高兴为你提供技术支持!
从原理图上看无法判断问题是来自硬件,建议先测试一下Jlink能否检测到内核(如下图所示)。
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------