Hello   I am gonna start working on a 56F8037 CPU, and I...

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hello   I am gonna start working on a 56F8037 CPU, and I...

Jump to solution
1,761 Views
AJPinotti
Contributor II
Hello
 
I am gonna start working on a 56F8037 CPU, and I just got from freescale a Trial License, so that I can compile more than 32KB. But I cannot find the CPU Bean at Processor Expert. This bean comes with the license or should I get another CW version.
 
Tks.
 
Alexandre
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
483 Views
ProcessorExpert
Senior Contributor III
Hello,

This CPU is supported only in the Processor Expert 2.98  and higher (Code Warrior 8.x). The newest version of CW and PE is possible to download here:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-56800E-DSC&nodeId=0127262E703BC3&f...

best regards
Vojtech Filip
Processor Expert Support Team
UNIS

View solution in original post

0 Kudos
Reply
2 Replies
483 Views
AJPinotti
Contributor II
I am using CodeWarrior IDE Version 5.6.1.1658 and CodeWarrior 568000/E Hybrid Controllers version 7.2.
 
Can someone help me?
 
Tks
0 Kudos
Reply
484 Views
ProcessorExpert
Senior Contributor III
Hello,

This CPU is supported only in the Processor Expert 2.98  and higher (Code Warrior 8.x). The newest version of CW and PE is possible to download here:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-56800E-DSC&nodeId=0127262E703BC3&f...

best regards
Vojtech Filip
Processor Expert Support Team
UNIS
0 Kudos
Reply