Hi~
I am developing with imx8mmevk now.
I succeeded cross-compile C file with imx8mmvek.
But I can't succeed c++ file now.
Anybody help me?
I did as below.
source /opt/fsl-imx-wayland/4.14-sumo/environment-setup-aarch64-poky-linux
aarch64-poky-linux-gcc --sysroot=$SDKTARGETSYSROOT -march=armv8-a -mcpu=cortex-a53 main.c
aarch64-poky-linux-g++ --sysroot=$SDKTARGETSYSROOT -march=armv8-a -mcpu=cortex-a53 main.cpp
To do cross-compile with C++, I added conf/local.conf and then I could see libstdc++.so.6 in /usr/lib as below.
But, the below error occurred now..
Hello,
Can you please try adding the "glibc" recipe to the IMAGE_INSTALL_append part in the local.conf and see if that solves the problem?
Best regards,
Diego.
Hi Diego~
Thank you for your reply.
I could success cross-compile C++ file with imx8mmvek after adding the below files.
But there was another problem.
Our application made for 32bit OS. We use pointer, array etc.
(Pointer 4byte in 32bit OS, Pointer 8 byte in 64bit)
So, if we want to use our application continuously without change source, could you let me know how should we do?
/usr/lib/libstdc++.so.6
/usr/lib/libstdc++.so.6.0.21
libgcc_s.so.1
Best regards,
Colin.