Hi community,
I have using 8MMINILPD4-EVK and FreeRTOS for Cortex-M4F. and I have some questions.
1. When debugging Cortex-M4F, do I need to set anything in the debugger script?
2. What configuration for Cortex-M4F is set by U-boot ?
I can build my application on DS-5 (armcc5), and I have run BIN file via u-boot command as follows.
If you use the ”fatload" command, the program will run without any problems.
u-boot=> fatload mmc 1:1 0x7e0000 XXXX_Cortex-M4F.bin
131764 bytes read in 11 ms (11.4 MiB/s)
u-boot=> bootaux 0x7e0000
## Starting auxiliary core at 0x007E0000 ...
u-boot=>
But I can not debug with 3rd party debugger(PATNER). When i use the 3rd party debugger, Interrupts (SVC, PendSVC, SysTick) were not occured.
Best Regards,
T.Kashiwagi
Solved! Go to Solution.
Hi Takashi
in general support with 3rd party debuggers may be provided with
NXP Professional Services | NXP
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor
Thank you for responding.
I'll contact the debugger developer.
Best Regards,
T.Kashiwagi
Hi Takashi
in general support with 3rd party debuggers may be provided with
NXP Professional Services | NXP
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------