How do I jtag debug Cortex-M4 with IMX8M mini?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How do I jtag debug Cortex-M4 with IMX8M mini?

Jump to solution
2,077 Views
Takashi_Kashiwagi
Senior Contributor I

Hi community,

I have using 8MMINILPD4-EVK and FreeRTOS for Cortex-M4F. and I have some questions.

1. When debugging Cortex-M4F, do I need to set anything in the debugger script?

2. What configuration for Cortex-M4F is set by U-boot ?

I can build my application on DS-5 (armcc5), and I have run BIN file via u-boot command as follows.

If you use the ”fatload" command, the program will run without any problems.

u-boot=> fatload mmc 1:1 0x7e0000 XXXX_Cortex-M4F.bin
131764 bytes read in 11 ms (11.4 MiB/s)
u-boot=> bootaux 0x7e0000
## Starting auxiliary core at 0x007E0000 ...
u-boot=>

But I can not debug with 3rd party debugger(PATNER). When i use the 3rd party debugger, Interrupts (SVC, PendSVC, SysTick) were not occured.

Best Regards,

T.Kashiwagi

Tags (3)
1 Solution
1,658 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

in general support with 3rd party debuggers may be provided with

NXP Professional Services | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
1,658 Views
Takashi_Kashiwagi
Senior Contributor I

Hi Igor

Thank you for responding.

I'll contact the debugger developer.

Best Regards,

T.Kashiwagi

0 Kudos
1,659 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

in general support with 3rd party debuggers may be provided with

NXP Professional Services | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------