Hello,
I have problems when I try to flash the IMXRT1050-EVBK, after debugging start the LED(D16) just flashing all the time and never stop, until "Terminate" button be clicked, and FW never be update. I tried couple examples code and I got the same thing.
IDE: MCUXpresso
EVB configuration:
- SW7: 1-off,2-on,3-off,4-on (Hyperflash in Serial Downloader mode)
- In J1, the header is placed on 3,4 (power for the board is supplied via USB at J9)
- In J27, the header is placed on 1,2
- USB cable is connected to J28
- USB cable is connected to J9
One more question: Can I use 512KB SRAM/TCM instead of external flash?
Thanks,
Carsoft
Hi Carsoft Lai,
Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
Q1) Please set SW7 ( 1-off,2-on,3-on,4-off) to assure boot from Hyper Flash.
Q2) Can I use 512KB SRAM/TCM instead of external flash?
-- Yes, you can, however, you need to remove the flash, then move SRAM_ITC up to the top as the Fig 1 illustrates.
Fig 1
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------