IPU Shutter for IMX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IPU Shutter for IMX6

638 Views
devikar
Contributor II

Hi,

We've set-up the Yocto BSP with 4.9.11-1.0 version for imx6qp-sabresd.

We need information about how to configure shutter for still image capturing.

Can you please give the direction for configuring shutter in device drivers.And also about SISG(Still Image Synchronization Generator). I have gone through the reference manual about SISG but did not understand where to enable MCU_ACTV_TRIG bit.

Thanks,

Devika

Labels (1)
0 Kudos
Reply
1 Reply

594 Views
igorpadykov
NXP Employee
NXP Employee

Hi Devika

description for these signals can be found in sect.37.5.2 SISG Control 0 Register (IPUx_SISG_CTRL0),

sect.37.4.12.8 SISG - Still Image Synchronization Generator i.MX6DQP Reference Manual

https://www.nxp.com/doc/IMX6DQPRM 

I am afraid there is no shutter support in BSPs.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply