Have a great day,
Yes there is System Version Register (SVR) which contains the system version number for the LS1022A. See section 12.3.10 System Version Register (DCFG_CCSR_SVR) in the LS1021A reference manual. The manual is available on page
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------