Product ID or System ID for the LS1022A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Product ID or System ID for the LS1022A

510 Views
amy_behrbaum
Contributor I

Is there a Product ID or System ID for the LS1022A?

Labels (1)
0 Kudos
1 Reply

408 Views
r8070z
NXP Employee
NXP Employee


Have a great day,

Yes there is System Version Register (SVR) which contains the system version number for the LS1022A. See section 12.3.10 System Version Register (DCFG_CCSR_SVR) in the LS1021A reference manual. The manual is available on page

https://www.nxp.com/products/processors-and-microcontrollers/arm-based-processors-and-mcus/qoriq-lay...

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos