Hi,
I try to use eSCI, port J20 on MPC5777C-416DS,to connect the freemaster, the program is debug and resume successfully, but the freemaster can't detect the board. what do I do wrong?In addition, I used to connect the EVB with freemaster in JTAG.
Thanks!
Hi,
1. select Dual wire mode in "esci" component
2. within freemaster _cfg.h use
#define FMSTR_USE_ESCI 1
instead of
#define FMSTR_USE_SCI 1
moreover disable TSA usage if table not defined in the code
#define FMSTR_USE_TSA 0
BR, Petr