Can't resume when the program suspended

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't resume when the program suspended

695 Views
490114602
Contributor I

Hi, 

Chip: MKE15Z256VLL7

MCUXpresso Version: 10.3.1

Debug Prober: SEGGER.   SWD mode

If I run the program without suspended or breakpoint, it runs no problem. But if I suspend it  manually or by setting a breakpoint, the program can not resume. It shows "Error: Command aborted." in debugger window. In Diassembly window shows "000018fc: Failed to execute MI command:
-data-disassemble -s 6396 -e 6428 -- 2
Error message from debugger back end:
Cannot access memory at address 0x18fc"

The code is running without FreeRTOS.

Thanks.

0 Kudos
Reply
1 Reply

591 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Ran Tao,

How about a simple project , for example "hello world" ?

And please step by step to check which code make it crash.


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply