Can zigbee experts give me some advice?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can zigbee experts give me some advice?

963 Views
yjvijfhvk
Contributor I

Dear friends,
I am a newcomer to the development of ZIGBEE, I should first look at what documents are better, and the software developed is downloaded there.

Labels (1)
0 Kudos
Reply
3 Replies

858 Views
patrick_pan
NXP Employee
NXP Employee

Hi, Liu

What kind of HW you will used for Zigbee development ? 

if you want to use KW , then you will use MCUXpresso to build App;

if you want to use JN , then you should use BeyondStudio for compiling 

0 Kudos
Reply

858 Views
yjvijfhvk
Contributor I
0 Kudos
Reply

858 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hi Liu,

Do you plan to use KW or JN for your application?, depending of this choise, I would suggest to check the SDK (KW) or the examples for the JN, in each of this package code there's some documentation you can check and some demo examples.

If you want to download the SDK, please check the following link and in the search bar, browse KW41Z:

Welcome | MCUXpresso SDK Builder 

For the examples, in the webpage you mention, please download first beyond studio. Also download the JN - AN - 1220 and  JN - AN - 1216, the first is an example for a sensor and the second is the control bridge that control the first one. This is a good example to start.

I hope this helps you.

 

Best Regards,

Alexis Andalon

0 Kudos
Reply