2.2 inch tft spi interface, low spi throughput

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2.2 inch tft spi interface, low spi throughput

2,366 Views
caglarabidin
Contributor I

Hi,

We are trying to interface 2.2 inch 320x240 tft screen via spi on imx6q(pico-pi-imx6). we are able to display video on the screen but we got 5 fps and ~1000KB/s throughput even at 30, 60 MHz spi clks. During the data transmission at high clock speeds, there is a  ~50 us gap between bursts. We believe this is the reason of the low  throughput. My question is how can we reduced the gap between the bursts. Is any modification  required to improve  throughput  for spi transmission? Is it possible to send   continuous  data with 30MHz or higher spi clocks?

Thanks in advance,

0 Kudos
Reply
3 Replies

1,009 Views
richardallen2
Contributor III

Are you using DMA or the CPU to drive the SPI?

0 Kudos
Reply

1,009 Views
caglarabidin
Contributor I

Hi Richard,

I enabled DMA  option in fbtft driver and checked DMAREG to confirm DMA is enabled.

0 Kudos
Reply

1,009 Views
igorpadykov
NXP Employee
NXP Employee

Hi caglar

max.spi clocks can be found in sect.4.12.2 ECSPI Timing Parameters i.MX6DQ Datasheet

http://www.nxp.com/docs/en/data-sheet/IMX6DQCEC.pdf

In general (if ecspi uses sdma) for reducing gaps one can try to tweak QoS using NIC-301,

described in Table 45-5. QoS and tidemark parameters i.MX6DQ Reference Manual

http://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply