LS1012 USB1_VBUS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1012 USB1_VBUS

564 Views
philbaron
Contributor I

What is the maximum tolerated voltage on the USB1_VBUS (pin 4) on the LS1012. Datasheets seems to imply that it is part of the 1.8V bank, but eval boards have this pin connected directly to VBUS which is 5V.

0 Kudos
2 Replies

495 Views
Bulat
NXP Employee
NXP Employee

USB1_VBUS is not a power pin, it is an input signal with nominal voltage of 5V. Please see the AN5192 for details.

Regards,

Bulat

0 Kudos

495 Views
philbaron
Contributor I

Bulat,

Thanks for the quick and concise response.

Phil Baron

Aeronix Inc.

777 Lowndes Hill Rd.

Bldg 3, Suite 160

Greenville, SC 29607

864-250-1950 x258

0 Kudos