How to configure and access the semc NAND flash?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to configure and access the semc NAND flash?

1,021 Views
zhangjiansheng
Contributor II

Hi,

In my board I use both the external SDRAM and the external NAND flash. They are both connected via semc. Is there any demo or example code to configure and operate the NAND flash?

I generate a SDK package from the NXP web site, and can't find the example for the NAND flash.

Thanks.

Tags (2)
0 Kudos
Reply
1 Reply

862 Views
jeremyzhou
NXP Employee
NXP Employee

Hi zhang jiansheng,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Unfortunately, there's no similar demo provided in the SDK library now, however, I'll report this request to the SDK team.
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply