Hello,
All eCSPI nodes in imx8mq.dtsi lack "dmas" and "dma-names" properties, see fsl-imx8mq.dtsi\freescale\dts\boot\arm64\arch - linux-imx - i.MX Linux kernel. As as result SPI DMA is disabled on i.MX8M. Is there any problem with SPI DMA on this platform ? The eCSPI controller on i.MX8M is the same as on i.MX6UL, but on i.MX6UL SPI DMA is enabled. I'd appreciate a clarification from NXP folks.
Thanks a lot.
Felix.
Hello,
Generally NXP BSP supports eCSPI DMA:
spi-imx.c\spi\drivers - linux-imx - i.MX Linux kernel
Accessing SPI Devices in Linux
Have a great day,
Yuri
------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer
button. Thank you!