In MacOS on MacBook and in Ubuntu 18.04 on PC LpcLink with CMSIS-DAP works OK. However, on the same machine in Windows 10, I get the following console output:
MCUXpresso IDE RedlinkMulti Driver v10.3 (Nov 28 2018 02:33:57 - crt_emu_cm_redlink build 748) Found part description in XML file nxp_lpc17xx.xme Reconnected to existing link server Connecting to probe 1 core 0 (using server started externally) gave 'Ee(42). Could not connect to core.' Connecting to probe 1 core 0 (using server started externally) gave 'Ee(42). Could not connect to core.' Connecting to probe 1 core 0 (using server started externally) gave 'Ee(42). Could not connect to core.' Server OK but no connection to probe 1 core 0 (after 3 attempts) - Ee(42). Could not connect to core. Failed on connect: Ee(42). Could not connect to core. No connection to chip's debug port
In the RedlinkServer console, I got the following:
probelist Index = 1 Manufacturer = NXP Semiconductors Description = LPC11U3x CMSIS-DAP v1.0.7 Serial Number = 0B023028 VID:PID = 1FC9:0132 Path = \\?\hid#vid_1fc9&pid_0132&mi_00#9&236ef90&0&0000#{4d1e55b2-f16f-11cf-88cb-001111000030} probestatus Index = 1 Manufacturer = NXP Semiconductors Description = LPC11U3x CMSIS-DAP v1.0.7 Serial Number = 0B023028 VID:PID = 1FC9:0132 Path = \\?\hid#vid_1fc9&pid_0132&mi_00#9&236ef90&0&0000#{4d1e55b2-f16f-11cf-88cb-001111000030} IsOpen = FALSE WireInitialized = FALSE WireProtocol = JTAG CoresConfigured = FALSE PacketSize = 64 Reference Count = 0 HasSWV = FALSE HasETM = FALSE HasJTAG = TRUE HasSWD = TRUE Probe Type = CMSIS-DAP Probe Reference Count = 0 probeopenbyindex 1 Probe not open
On the same PC, the probe works in virtual machine as well..
What shall I do?
Reinstalling Windows solved the problem..