I would like to use mobile SDRAM if possible with the RT1060 (such as Micron MT48H32M16LFB4-6 IT). I see the GPIO block for the memory has a seperate power input. If I supply this with 1.8V will this work? Also how would I set the extended mode register?
Q. If I supply this with 1.8V will this work?
A. Yes, it will work.
Q. Also how would I set the extended mode register?
A. The only difference between the Set Mode Register and Set Extended Mode Register commands is that for the first one the address pattern should be selected so as both Bank Address BA1 and BA0 signals are 0, whereas for the second one BA1 should be 0 and BA0 should be 1. So, you only have to select the appropriate address pattern with BA1=0 and BA0=1 when executing the Set Mode Register command to access the extended mode register.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------