I am using MQX4.1 with Codewarrior V10.6.4 and most of the projects I work on are K60 based designs.
We purchase a TWR-K60D100M kit and use the BSP for this board set as the starting point for our custom boards.
Using the cloning BSP I create a new board BSP.
I create a new Workspace for each new project and copy the .wsd files generated by the cloning wizard into the new work space and the .xml file into the CodewarriorNPW directory. I then build the libraries (sometimes this requires one or two passes which is a little worrying ) and then create a new project and and select the new-board BSP. The project creates fine and I can compile the new new project without errors.
But, when I want to make a change to the BSP - say within the config.h file, although the file I open is the one in the project workspace, I think the file that actually gets changed is the one created by the cloning BSP and not the one I have copied into the current workspace.
Can someone please explain why the is and if there has been a change to the working of these directories for I am sure that projects I have worked on in the past have allowed me to make changes to the BSP in the local workspace and not what might be described the global one.
Thanks
Ken
Hi Ken:
.wsd file is simple xml file describing project dependencies.
I would suggest you read Getting Started with Freescale MQX BSP Cloning wizard for how to clone a MQX BSP.
Regards
Daniel