Hi Rich,
i read ur solution and found very helpful ,also try it but never success or i can say i'm confuse.
I compile and flash the program (MCF52233 ), which shows... paste S19 upgrade file now...
on hyperterm. How can i put student.s19 ? i'll try it using hyperterm send file but with no success..
can u put more light on this??
Once it says to paste the S19 file, you're in the home stretch!
Just open the (student) S19 file in notepad, select Edit->Select All, and then Edit->Copy.
Then go back to HyperTerminal and select Edit->Paste To Host.
The student S19 should load, reset, and then run.
-- Rich
Thanks Rich ,
I really dont click this , but still i hv no success. i hv mcf52233DEMO board , is there are any jumper setting or something
that i cant feagure it out? When i paste image onto it , gives message like record not found.
It is also really helpful to everyone if u point out link which described S19 image description i.e how to decode it?
If when you paste the S19 into the terminal emulator, you get an error indicating a bad record format, you're almost there...
You can see the record format that is expected in the sources/flash.c file, in the routine flash_download().
Your S19 file should look like the one in bin/student.elf.S19 (in your zip file), starting and ending with similar lines.
Again, you want to open the S19 in notepad, Ctrl-A, Ctrl-C, and then paste the result into the hyperterminal window. You might have to step thru with the debugger if you're getting a format error and see exactly why... It will also help if you post the exact error message (you can also find it in flash.c and figure out what is up from there).
Have you tried pasting the student.elf.S19 file directly from the zip?
-- Rich
sorry rich ,
sorry for so late reply ,thanks for ur patience.
and now i got it.
thanks once again.