What should be the correct power to VDDSOC_IN & VDDARM_IN ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What should be the correct power to VDDSOC_IN & VDDARM_IN ?

593 Views
peteramond
Contributor V

Hi All,

I can see in Nitrogen 6 max & sabre lite boards have used 1.2V for VDDSOC_IN, VDDARM_IN and VDDARM23_IN of the iMX6Q processor. But it is 1.375V in Freescale SabreSD board. What should be the correct voltage for this ?

Can anyone tell me the recommended voltages for processor power blocks ?

Nitrogen6_max

pastedImage_1.png

Sabre SD

pastedImage_2.png

Regards,

Peter.

Labels (3)
0 Kudos
Reply
1 Reply

471 Views
igorpadykov
NXP Employee
NXP Employee

Hi Peter

for i.MX6Q it is defined in Table 6. Operating Ranges i.MX6DQ Datasheet

http://www.nxp.com/docs/en/data-sheet/IMX6DQCEC.pdf

and sect.8.4.3 Clocks at boot time i.MX6DQ Reference Manual

http://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf

For other i.MX processors - in their datasheets.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply