Hi ,
Trying to use the MCIMX7 SABRE 700-28590 REV D board .using the bundle 342-00659 REV B1 sdcard which is having 4.1.15_2.0.1 B version getting GUI image on HDMI display .But when tried to build image using imx-4.9.88-2.0.0_ga not getting GUI ON HDMI,but can see embedded linux splash and progress bar ,but no GUI after that .Followed all the instructions as per latest bundled documents and read me.Also tried setting bootargs also.Please help to fix resolve this issue.
Please suggest a fix/solution for the issue . How to get HDMI working.Following are the details
[board]
MCIMX7 SABRE 700-28590 REV D
[BSP]
4.9.88-2.0.0_ga: ROCKO
[build option]
MACHINE=imx7dsabresd
DISTRO=fsl-imx-xwayland
[build target]
fsl-image-validation-imx
Thanks,
Sam