imx7 sabre no hdmi output

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx7 sabre no hdmi output

955件の閲覧回数
syamkrishnan_m
Contributor II

Hi ,

Trying to use the  MCIMX7 SABRE  700-28590 REV D board .using the bundle 342-00659 REV B1 sdcard which is having 4.1.15_2.0.1 B version  getting GUI image on HDMI display .But when tried to build image using imx-4.9.88-2.0.0_ga not getting GUI ON HDMI,but can see embedded linux splash and progress bar ,but no GUI after that .Followed all the instructions as per latest bundled documents and read me.Also tried setting bootargs also.Please help to fix resolve this issue.

Please suggest a fix/solution for the issue . How to get HDMI working.Following are the details

[board]

MCIMX7 SABRE  700-28590 REV D

[BSP]

4.9.88-2.0.0_ga: ROCKO

 

[build option]

MACHINE=imx7dsabresd

DISTRO=fsl-imx-xwayland

 

[build target]

fsl-image-validation-imx


Thanks,

Sam

ラベル(1)
0 件の賞賛
3 返答(返信)

846件の閲覧回数
syamkrishnan_m
Contributor II

Please suggest a fix/solution for the issue . How to get HDMI working.

Thanks

0 件の賞賛

846件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Syam,

Try to connect serial port, maybe you are receiving an error, because HDMI should work.

Regards

0 件の賞賛

846件の閲覧回数
syamkrishnan_m
Contributor II

Hi Alfred Soto,

Thanks for the reply.

I didnt get any error in console output.Is there any settings need to be changed in hardware or software to enable HDMI.

Thanks ,

Syam

0 件の賞賛