Re: iMX6 on-die temperature measurement

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Re: iMX6 on-die temperature measurement

916 Views
wangwenxue1989
Contributor I

hi Yuri,

For industrial level chip(-40--105),if I set this value to 95,does it have risks?

Best Regards,
Wenxue

0 Kudos
Reply
1 Reply

716 Views
Yuri
NXP Employee
NXP Employee

Hello,

  I think it is possible to use the value of 95 degree C (as highest possible).

Please refer also to app note AN5215.

https://www.nxp.com/docs/en/application-note/AN5215.pdf 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply