Hi ,
I am trying to flash my MCIMX512CJM6C in advanced toolkit through usb port in mode HAB
But i am getting an error "No usb detected"
I have made usb type a connection as below
but IMX512 is detecting in my pc in device manager it listing as SE Blank Elvis
is there any driver needs to be installed to detect imx512?
Please help me out to detect my imx512 to flash
Regards,
Arun
i could make it work with windows XP but its doesnot work with windows 7
Hi Arunprasath
one can check usb recommendations in Chapter 22 Porting USB Host1 and USB OTG
https://www.nxp.com/docs/en/user-guide/MX53UG.pdf
Try with i.MX53 QSB board or with mfg tool on
i.MX537 Processors|HD Video|NXP
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
I have access to only
Regards,
Arun
Hi Arunprasath
it should work with that configuration. Also one can connect through usb hub.
Best regards
igor
Hi Igor,
the above connection is enough? in that case why in device manager it listing as SE Blank Elvis
Regards,
Arun
Hi Arunprasath
USB_OTG_ID does not require any connection.
Best regards
igor
Hi Igor,
then why in device manager it listing as SE Blank Elvis?
Do i need to install any driver?
Regards,
Arun
Hi Arunprasath
"SE Blank Elvis" is message provided by ROM,
in general you can ignore it. No need to install additional drivers.
Best regards
igor