Hi, I have a trouble with MCUXpress.
I have a K60D100M board. I've installed MCUXpresso IDE v10.2.0 [Build 759] [2018-05-15] on Linux Ubuntu 16.04.4 LTS.
When I look for my board, it show me: "No compatible probes available. They may be disabled, disconnected, not powered, already in use or not compatible with this target"
I have installed necessary drivers (pemicro-other-20170809-linux64.zip.tar.gz)
I look for my board and I find it next:
I have created a VM with WIN7, install the same version of MCUXpresso IDE, and they are working fine.
How do I make the board work also in ubuntu ?
thank you!
Hi Daniel.
Do you use TWR-K60D100M board with on board P&E OSJTAG interface? what's it version?
Can you try another USB interface, and create a new project in a new workspace to test this connection?
Best Regards
Jennie Zhang