imx6d can't work well when using two capture interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6d can't work well when using two capture interface

Jump to solution
1,137 Views
leihe
Contributor I

the single comes from ds90ub940 and adv7180 ,ds90ub940 config is ipu0、csi1、VC1,adv7180 config is ipu0、csi0、VC0,if  ds90ub940's FPDlink is disconnected this two video will lost. this two video device can work well along .can somebody help me thank you.

Labels (6)
0 Kudos
Reply
1 Solution
925 Views
igorpadykov
NXP Employee
NXP Employee

Hi lei

may be helpful to look at several cameras example on

iMX6DQ MAX9286 MIPI CSI2 720P camera surround view solution for Linux BSP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
926 Views
igorpadykov
NXP Employee
NXP Employee

Hi lei

may be helpful to look at several cameras example on

iMX6DQ MAX9286 MIPI CSI2 720P camera surround view solution for Linux BSP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------