I just installed "BeyondStudio for NXP", then installed the "JN516x IEEE 802.15.4 SDK", then imported the JN-AN-1174 project, but when I build it, I get tons of errors because of unresolved definitions. Are there additional entities that need to be imported into the Workspace in order to successfully build this project? Are there special path specifications required? I've followed all the instructions for the SDK and the JN-AN-1174. I expected it to build... Any help is appreciated - thanks! (Screenshot included).
I cleared the errors and rebuit and now it seems to build OK and reports no errors. Not sure why the errors appeared initially. Any ideas about that? It seems to be building without errors now...
Hi Matt,
Could you please look at the next community document?
Please let me know if you have further questions.
Regards,
Mario