Hi.
On https://mcuxpresso.nxp.com/en/select there are two boards for RT1050:
EVK-MIMXRT1050, with "KSDK 2.3.0 (released 2018-01-11)"
EVKB-IMXRT1050, with "KSDK 2.4.0 (released 2018-05-25)"
Will EVK-A be updated to 2.4.0?
Hi Mike,
Yes, the KSDK 2.4.0 can work on KSDK 2.4.0 board. Both this two version BSP can work on EVK-A. But EVKB-IMXRT1050 only support KSDK 2.4.0.
Have a great day,
Rita
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------