I'm trying to set up an i.MX_7Dual Sabre board for with the FreeRTOS BSP. I'm trying to run a blinking lights demo application. I'm at the point where I've connected to the board's serial debug port and am using a serial terminal (in my case PuTTY on Windows 10) in order to run the demo's binary file via TCM. However, when I start up the serial connection, I get no serial messages from the board at all and it doesn't seem to boot up. PuTTY still recognizes that there is serial connected and the board's debug LED's light up when I send keystrokes from the terminal, but not much else.
Hi Chris
one can check sect.6.1 Running application on TCM (Cortex-M4 Core's Tightly
Coupled Memory) with U-Boot attached Getting_Started_with_FreeRTOS_BSP_for_i.MX_7Dual.pdf
and pay attention to TTY devices on Figure 25. Determining the COM Port of target board.
Demo Images can be found on
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------