Can all jtag pins leave floating if they are not used?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can all jtag pins leave floating if they are not used?

1,127 Views
sunjianxin66
Contributor II

Dear NXP

I am not using the jtag functions on IMX6(scm-imx6q). Can I float all of them? or is there a proper way connects all those 6 jtag pins (screen shot attached) for disabled jtag.

Thank you very much!

Jianxin

Labels (2)
Tags (2)
0 Kudos
Reply
1 Reply

934 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Jianxin,

You can see the schematic of SCM-i.MX6Q, if you do not use the JTAG you can not float all of them.

JATG PIN.PNG

You need to do the following actions before float them. Then you can connect them separately to test mode.

PU(10K)

JTAG_TMS

JTAG_TDI

Pull UP JTAG_nTRST to high votage

PD(4.7K)

JTAG_MOD

JTAG_TCK and JTAG_TDO can directly floating.
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply